Hi, I'm able to compile and run the Usb_Dev_Bulk from f28m35 v201of controlsuite3.2.4 using CCS-v5.5 on Development Kit(TMDXCNCDH52C1) . But my Win XP SP3 does not able to detect the USB device correctly after restart. The steps of set up are below:
1) i load the Usb_Dev_Bulk .out to flash using ccs5.5 .and i run the program,system can detect generic bulk device immediately.
2) i Power off and restart the kit.and Windows XP SP3 detect it very slowly and finally name it "Unknown Device" under USB controller.
3) vid and pid are 0 of the "Unknown Device".i think the device is not Successful enumeration .
how to slove the problem?
thanks ,bao.