Hi,
I am having some trouble running a project on a F28062. I ran an example project which runs from flash. I didnt have any interrupts enabled but for some reason my processor halted at a reserved ISR (rsvd_isr).
Now when I try launch another debug session I get an error saying that I cannot connect to target.
C28xx: Error: (Error -1135 @ 0x39B2BD) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.0.471.0)
C28xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
Does anyone have any idea as to why this is happening. I would appreciate any help.
Thanks
Faizan