This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

the problem about PLC G3

Other Parts Discussed in Thread: MSP430F5419A, TMS320F28069

Hi All

I'm development intelligient lighting product with PLC G3,i have completed HCT

protocol over MSP430F5419A,and G3 management client and event monitor client on

DC over AM335x.To be able to communication with each other(between client and

DC),i followed

below steps.

1)client initialized some config.

2)client run discover network,and received response with PAN ID from DC

3)client attached to DC with returned PAN ID

4)the detach command was sent to event monitor client first,and attach command

was sent toevent monitor client secondly by DC.in the attach command,the short

address and ext address were sent.the ext address was the same with client

setting,but short address was changed during diffrent attach.so I do not

understand a lot of problems about G3,the detail is described as bellow.

1)according to unicast communication,DC using ipv6 address to address device,

ipv6 address is composed of short address and PAN ID,please refer to attached image

,but short address is not fixed,so how can DC access the same client during different attch?



2)on the client side,i can just only set long address,the short address

is allocated dynamically by DC,so how to realize the unique addressing?

3)Is long address the same with ext address?if not,how to map long address

to ext address?

4)During communication,how can DC know received data is come from witch

client?  because i can not get the client's address.

5)If mutilcast is used,how is the group address created and set?Is the client

wicthit is not included in the group address able to receive data?how client is

able to receive data during multicast?