Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed: 5.2.3 [C2000]. Another version of the compiler will be used during build: 6.1.3. Please install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties. Lab9 properties Problems