Hi, I am having problem with the DSP i am using for my project. I am using F28335. And the encoder i am using it is open collector type. My output from the encoder is fine. It is giving pulses to the input of the DSP. I have checked the input pins for QEP1A, QEP1B. The pulses are there. But, after the running the program it is not giving the electrical theta and the RPM value. Note that, this problem is happening with the mini module of TI DSP F28335. Then i checked the program with another Experimenter’s Kit USB Docking Station i have. The program is working fine in that kit and getting all the desired value.
Please suggest me what i can do for the mini module i using right now.