Hi,
I am running my VnV tests on eZDSP F28335 Digital spectrum board. Actually i am running my tests through RTRT tool. And i m using CCS V5.3 compiler. When i run my test node in RTRT the test is getting compiled but it is not getting connected to the target. It is saying "Error Initializing Emulator".
I tried both USB and JTAG to interface the target board and PC. But it is giving the same problem. So many times i tried to reset the hardware, but it is not working.
Can anybody pls help me on this?
Regards,
Iswarya