This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issue with compiler for a F28035

Hi all,

So I am a little new to embedded programming.  I am working with a F28035 chip and using Code Composer studio 5.1 to develop software.  I am trying to build my project, and found I am getting this error:

Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed: 6.1.4 [C2000]. Another version of the compiler will be used during build: 6.1.3. Please install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties. DSP28035-empty properties TI Problem Marker

This project used to build, when I was using Code Composer 5.4.  I downgraded because I was having an issue with an ARM compiler.  When I reverted, this code stopped working.  I have gone through the Install New Software, and am on the C2800 6.1.6 version.  I also have the 6.0.6 version installed.  Any help on getting this project up and running would be great.

Thanks,

Seth