This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to run "boot to Flash" boot loader mode for F28035 after a reset

I am using a custom board. I can install the code and then remove the JTAG connection, the F28035 works great.  After resetting the power to the processor, the whole code is not working..

Attached is my .cmd file. Do you have any suggestion to boot from Flash? 

A TI documentation is also appreciated.

 

_Cla1Prog_Start = _Cla1funcsRunStart;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start


MEMORY
{
/*Program Space*/
PAGE 0:
RAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM (L0)*/
RAML3 : origin = 0x009000, length = 0x001000 /* data RAM (L3) */
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASHH : origin = 0x3E8000, length = 0x002000 /* on-chip FLASH */
FLASHG : origin = 0x3EA000, length = 0x002000 /* on-chip FLASH */
FLASHF : origin = 0x3EC000, length = 0x002000 /* on-chip FLASH */
FLASHE : origin = 0x3EE000, length = 0x002000 /* on-chip FLASH */
FLASHD : origin = 0x3F0000, length = 0x002000 /* on-chip FLASH */
FLASHC : origin = 0x3F2000, length = 0x002000 /* on-chip FLASH */
FLASHA : origin = 0x3F6000, length = 0x001F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */

IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */

BOOTROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */

/*Data Space*/
PAGE 1 :
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
CLARAM0 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */
CLARAM1 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */
CLA_CPU_MSGRAM : origin = 0x001480, length = 0x000080 /* CLA-R/W, CPU-R message RAM */
CPU_CLA_MSGRAM : origin = 0x001500, length = 0x000080 /* CPU-R/W, CLA-R message RAM */

FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */

}


SECTIONS
{
/* Allocate program areas: */
// .cinit : > FLASHA, PAGE = 0
// .pinit : > FLASHA, PAGE = 0
// .text : > FLASHA, PAGE = 0

.cinit : > FLASHE, PAGE = 0
.pinit : > FLASHE, PAGE = 0
.text : > FLASHE|FLASHF|FLASHH, PAGE = 0

codestart : > BEGIN PAGE = 0

ramfuncs : LOAD = FLASHD,
RUN = RAML0,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0

Cla1Prog : LOAD = FLASHC, /* Note for running from RAM the load and RUN can be the same */
RUN = RAML3,
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
PAGE = 0



csmpasswds : > CSM_PWL PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0

/* Allocate uninitalized data sections: */
.stack : > RAMM0, PAGE = 1
.ebss : >> RAMM0|RAMM1|CLARAM1, PAGE = 1
.esysmem : > RAMM1, PAGE = 1

/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHA PAGE = 0
.switch : > FLASHA PAGE = 0

/* Allocate IQ math areas: */
IQmath : > FLASHD PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */

Cla1ToCpuMsgRAM : > CLA_CPU_MSGRAM PAGE = 1
CpuToCla1MsgRAM : > CPU_CLA_MSGRAM PAGE = 1

ClaDataRam0 : > CLARAM0, PAGE = 1
ClaDataRam1 : > CLARAM1, PAGE = 1
CLAmathTables : > CLARAM1, PAGE = 1
CLA1mathTables : > CLARAM1, PAGE = 1

//
// Must be allocated to memory the CLA has write access to
//
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > CLARAM0, PAGE = 1

.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT

}