Hi
i am using c2000 launch pad(F28027) to generate complementary pwm with dead band. These pulses are used to drive the mosfets in DC-DC converter. one of the mosfet is at low side and another is at higher side. I am using isolated gate driver with isolated power supply to drive these mosfets. SL7407 buffer ic is used between c2000 launch pad and and opto coupler . Launch pad is powered through usb cable .I am getting following error when i am increasing my input voltage of the dc to dc converter from 12V to 24V.
"C28xx: Error: (Error -150 @ 0x0) One of the FTDI driver functions used during configuration returned a invalid status or an error. (Emulation package 5.1.73.0)"- Please tell me how to overcome this problem.
Regards
shelas sathyan