Other Parts Discussed in Thread: TMS320F28027, CONTROLSUITE
Hi friend ,
I have return eeprom interface with c2000 TMS320F28027 through i2c . I have problem in read and write please any one help me
this is my code...
while(I2caRegs.I2CSTR.bit.XRDY == 0){};
I2caRegs.I2CDXR = *txBuf_pu8;
}
void i2cRead(Uint16 memAddr_u16, unsigned char *rxBuf_pu8, Uint32 rxDataLen_u32)
{
Uint32 i = 0;
I2caRegs.I2CSAR = I2C_SLAVE_ADDR; //Set slave address
I2caRegs.I2CCNT = 2; //Set count to 2 address bytes
I2caRegs.I2CDXR =((memAddr_u16 >> 8) & 0xFF); //Send eeprom high address
I2caRegs.I2CMDR.bit.TRX = 1; //Set to Transmit mode
I2caRegs.I2CMDR.bit.MST = 1; //Set to Master mode
I2caRegs.I2CMDR.bit.FREE = 1; //Run in FREE mode
I2caRegs.I2CMDR.bit.STP = 0; //Dont release the bus after Tx
I2caRegs.I2CMDR.bit.STT = 1; //Send the start bit, transmission will follow
while(I2caRegs.I2CSTR.bit.XRDY == 0){}; //Do nothing till data is shifted out
I2caRegs.I2CDXR = ( memAddr_u16 & 0xFF ); //Send eeprom low address
I2caRegs.I2CCNT = rxDataLen_u32; //read 5 bytes from eeprom
I2caRegs.I2CMDR.bit.TRX = 0; //Set to Recieve mode
I2caRegs.I2CMDR.bit.MST = 1; //Set to Master mode
I2caRegs.I2CMDR.bit.FREE = 1; //Run in FREE mode
I2caRegs.I2CMDR.bit.STP = 1; //Stop when internal counter becomes 0
I2caRegs.I2CMDR.bit.STT = 1; //Repeated start, Reception will follow
for(i = 0; i < rxDataLen_u32; i++)
while(I2caRegs.I2CSTR.bit.RRDY == 0){}; //I2CDRR not ready to read?
*rxBuf_pu8 = I2caRegs.I2CDRR;
rxBuf_pu8++;
}
}
void main(void)
{
Uint16 address = 0x0005;
unsigned char txdata = 'H';
unsigned char rxdata = 0;
InitSysCtrl();
InitI2CGpio();
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
i2cInit();
EINT;
i2cWrite( address, &txdata, 1);
while(1)
{
i2cRead( address, &rxdata, 1);
}
}