This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ecap inputs in f28m35h52f1problem

using pins 6,8,32,43,45 as ecap input in coresponding to ecap6,ecap5,ecap3,ecap1,ecap2 i cane musure 5 diferent PWM inputs. the mesuerment is very exact.

However, the signals are coming from radio transmiter and if the antena is close to the board (1 meter) the 5 ecaps show 0. when i look at the input signals on the ecap pins i see them clean and nice like ttl signals shuld be. (1-2 milisecond Hight 70 herz signals)

the signals are entering to the board via 74lcx244 buffer.

need advice since it is amazing.

Tsfania

  • Hi, Tsfania.

    Tsfania Tsalisher said:

    However, the signals are coming from radio transmiter and if the antena is close to the board (1 meter) the 5 ecaps show 0. 

    It sounds as if the board was at the minimum of a diffraction Fresnel zone ;-). Clarify, please, how you check your eCAPs (where you see "0", with what tool?), i.e. what do you mean under "the 5 ecaps show 0"?

    Regards,

    Igor