This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPIO pin does not work to be set - Delfino (C28346)

Hi!

In my program I want to set the state of GPIO pins. But there are some circumstances which lead to the result that a pin register is not set to the correct state.

e.g.

GpioDataRegs.GPCDAT.bit.GPIO64 = 0   (result: 0)


GpioDataRegs.GPCDAT.bit.GPIO65 = 0   (result: 0)

GpioDataRegs.GPCDAT.bit.GPIO68 = 1   (result: 1)

GpioDataRegs.GPCDAT.bit.GPIO67 = 1   (result: 0)

GpioDataRegs.GPCDAT.bit.GPIO66 = 1   (result: 1)

This result is only generated if the program runs, if the debugger is used and the instructions are stepped over everything is set correctly as in source code.

I found out that inserting a NOP between every instruction does not change anything. But writing the same instruction doubled to the source line generates a correct result.


Isn't it allowed to use the bit registers in consecutive instructions?

what else could be the problem?

The CPU is clocked at 300MHz

Compiler Version: c2000_6.1.0

Code Composer Version:  5.3.0.00090

thanks for your help!