This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

eCANA interfacing between two uC f28069

Other Parts Discussed in Thread: TMS320F28069, ISO1050

Hi All,


I am interfacing two custom boards with TMS320F28069 using eCAN for data exchange. The back2back example from the control suite is running fine on both of them, but when I am connecting it thro' transciever ISO1050 there seems to be no activity. The Rx loops hangs on at "while(ECanaRegs.CANRMP.all != 0xFFFFFFFF ) {}  // Wait for all RMPn to be set.. " and the Tx loops on the other board hangs at "while(ECanaRegs.CANTA.all != 0xFFFFFFFF ) {}  // Wait for all TAn bits to be set.. ". I have also made sure that reciever runs before the trasmitter.

The example ecan_back2back has been modified for testing and is attached here. Can somebody help me in pointing out the mistakes.


thanks

Balwant

#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

//#define _RCV_

// Prototype statements for functions found within this file.
void mailbox_check(int32 T1, int32 T2, int32 T3);
void mailbox_read(int16 i);

// Global variable for this example
Uint32  ErrorCount;
Uint32  PassCount;
Uint32  MessageReceivedCount;
Uint32  MessageSendCount;

Uint32  TestMbox1 = 0;
Uint32  TestMbox2 = 0;
Uint32  TestMbox3 = 0;

void main(void)
{

    Uint16  j;


   struct ECAN_REGS ECanaShadow;

   InitSysCtrl();


   InitECanGpio();

   DINT;

   InitPieCtrl();


   IER = 0x0000;
   IFR = 0x0000;


   InitPieVectTable();


    MessageSendCount = MessageReceivedCount = 0;
    ErrorCount = 0;
    PassCount = 0;

    InitECana(); // Initialize eCAN-A module

    // Mailboxs can be written to 16-bits or 32-bits at a time
    // Write to the MSGID field of TRANSMIT mailboxes MBOX0 - 15

    ECanaMboxes.MBOX0.MSGID.all = 0x9555AAA0;
    ECanaMboxes.MBOX1.MSGID.all = 0x9555AAA1;
    ECanaMboxes.MBOX2.MSGID.all = 0x9555AAA2;
    ECanaMboxes.MBOX3.MSGID.all = 0x9555AAA3;
    ECanaMboxes.MBOX4.MSGID.all = 0x9555AAA4;
    ECanaMboxes.MBOX5.MSGID.all = 0x9555AAA5;
    ECanaMboxes.MBOX6.MSGID.all = 0x9555AAA6;
    ECanaMboxes.MBOX7.MSGID.all = 0x9555AAA7;
    ECanaMboxes.MBOX8.MSGID.all = 0x9555AAA8;
    ECanaMboxes.MBOX9.MSGID.all = 0x9555AAA9;
    ECanaMboxes.MBOX10.MSGID.all = 0x9555AAAA;
    ECanaMboxes.MBOX11.MSGID.all = 0x9555AAAB;
    ECanaMboxes.MBOX12.MSGID.all = 0x9555AAAC;
    ECanaMboxes.MBOX13.MSGID.all = 0x9555AAAD;
    ECanaMboxes.MBOX14.MSGID.all = 0x9555AAAE;
    ECanaMboxes.MBOX15.MSGID.all = 0x9555AAAF;

    // Write to the MSGID field of RECEIVE mailboxes MBOX16 - 31
    ECanaMboxes.MBOX16.MSGID.all = 0x9555AAB0;
    ECanaMboxes.MBOX17.MSGID.all = 0x9555AAB1;
    ECanaMboxes.MBOX18.MSGID.all = 0x9555AAB2;
    ECanaMboxes.MBOX19.MSGID.all = 0x9555AAB3;
    ECanaMboxes.MBOX20.MSGID.all = 0x9555AAB4;
    ECanaMboxes.MBOX21.MSGID.all = 0x9555AAB5;
    ECanaMboxes.MBOX22.MSGID.all = 0x9555AAB6;
    ECanaMboxes.MBOX23.MSGID.all = 0x9555AAB7;
    ECanaMboxes.MBOX24.MSGID.all = 0x9555AAB8;
    ECanaMboxes.MBOX25.MSGID.all = 0x9555AAB9;
    ECanaMboxes.MBOX26.MSGID.all = 0x9555AABA;
    ECanaMboxes.MBOX27.MSGID.all = 0x9555AABB;
    ECanaMboxes.MBOX28.MSGID.all = 0x9555AABC;
    ECanaMboxes.MBOX29.MSGID.all = 0x9555AABD;
    ECanaMboxes.MBOX30.MSGID.all = 0x9555AABE;
    ECanaMboxes.MBOX31.MSGID.all = 0x9555AABF;


    // Configure Mailboxes 0-15 as Tx, 16-31 as Rx
    // Since this write is to the entire register (instead of a bit
    // field) a shadow register is not required.
    //ECanaRegs.CANMD.all = 0xFFFF0000;

#ifdef _RCV_
    ECanaShadow.CANMD.all = ECanaRegs.CANMD.all;
    ECanaShadow.CANMD.all = 0xFFFFFFFF;
    ECanaRegs.CANMD.all = ECanaShadow.CANMD.all;
#else
    ECanaShadow.CANMD.all = ECanaRegs.CANMD.all;
    ECanaShadow.CANMD.all = 0x00000000;
    ECanaRegs.CANMD.all = ECanaShadow.CANMD.all;
#endif

    // Enable all Mailboxes */
    // Since this write is to the entire register (instead of a bit
    // field) a shadow register is not required.
    ECanaShadow.CANME.all = ECanaRegs.CANME.all;
    ECanaShadow.CANME.all = 0xFFFFFFFF;
    ECanaRegs.CANME.all = ECanaShadow.CANME.all;

    // Specify that 8 bits will be sent/received
    ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX1.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX2.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX3.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX4.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX6.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX7.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX8.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX9.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX10.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX11.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX12.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX13.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX14.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX16.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX17.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX18.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX19.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX20.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX21.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX22.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX23.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX24.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX25.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX26.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX27.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX28.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX29.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX30.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX31.MSGCTRL.bit.DLC = 8;

    // Write to the mailbox RAM field of MBOX0 - 15

    ECanaMboxes.MBOX0.MDL.all = 0x9555AAA0;
    ECanaMboxes.MBOX0.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX1.MDL.all = 0x9555AAA1;
    ECanaMboxes.MBOX1.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX2.MDL.all = 0x9555AAA2;
    ECanaMboxes.MBOX2.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX3.MDL.all = 0x9555AAA3;
    ECanaMboxes.MBOX3.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX4.MDL.all = 0x9555AAA4;
    ECanaMboxes.MBOX4.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX5.MDL.all = 0x9555AAA5;
    ECanaMboxes.MBOX5.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX6.MDL.all = 0x9555AAA6;
    ECanaMboxes.MBOX6.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX7.MDL.all = 0x9555AAA7;
    ECanaMboxes.MBOX7.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX8.MDL.all = 0x9555AAA8;
    ECanaMboxes.MBOX8.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX9.MDL.all = 0x9555AAA9;
    ECanaMboxes.MBOX9.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX10.MDL.all = 0x9555AAAA;
    ECanaMboxes.MBOX10.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX11.MDL.all = 0x9555AAAB;
    ECanaMboxes.MBOX11.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX12.MDL.all = 0x9555AAAC;
    ECanaMboxes.MBOX12.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX13.MDL.all = 0x9555AAAD;
    ECanaMboxes.MBOX13.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX14.MDL.all = 0x9555AAAE;
    ECanaMboxes.MBOX14.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX15.MDL.all = 0x9555AAAF;
    ECanaMboxes.MBOX15.MDH.all = 0x89ABCDEF;


    ECanaMboxes.MBOX16.MDL.all = 0x9555AAB0;
    ECanaMboxes.MBOX16.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX17.MDL.all = 0x9555AAB1;
    ECanaMboxes.MBOX17.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX18.MDL.all = 0x9555AAB2;
    ECanaMboxes.MBOX18.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX19.MDL.all = 0x9555AAB3;
    ECanaMboxes.MBOX19.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX20.MDL.all = 0x9555AAB4;
    ECanaMboxes.MBOX20.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX21.MDL.all = 0x9555AAB5;
    ECanaMboxes.MBOX21.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX22.MDL.all = 0x9555AAB6;
    ECanaMboxes.MBOX22.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX23.MDL.all = 0x9555AAB7;
    ECanaMboxes.MBOX23.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX24.MDL.all = 0x9555AAB8;
    ECanaMboxes.MBOX24.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX25.MDL.all = 0x9555AAB9;
    ECanaMboxes.MBOX25.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX26.MDL.all = 0x9555AABA;
    ECanaMboxes.MBOX26.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX27.MDL.all = 0x9555AABB;
    ECanaMboxes.MBOX27.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX28.MDL.all = 0x9555AABC;
    ECanaMboxes.MBOX28.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX29.MDL.all = 0x9555AABD;
    ECanaMboxes.MBOX29.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX30.MDL.all = 0x9555AABE;
    ECanaMboxes.MBOX30.MDH.all = 0x89ABCDEF;

    ECanaMboxes.MBOX31.MDL.all = 0x9555AABF;
    ECanaMboxes.MBOX31.MDH.all = 0x89ABCDEF;

   

    // Since this write is to the entire register (instead of a bit
    // field) a shadow register is not required.
    EALLOW;
    ECanaRegs.CANMIM.all = 0xFFFFFFFF;

    // Configure the eCAN for self test mode
    // Enable the enhanced features of the eCAN.
    EALLOW;
    ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
    ECanaShadow.CANMC.bit.STM = 0;    // Configure CAN for self-test mode
    ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;

    EDIS;

    // Begin transmitting
    for(;;)
    {


#ifdef _RCV_
        while(ECanaRegs.CANRMP.all != 0xFFFFFFFF ) {}  // Wait for all RMPn to be set..

        ECanaRegs.CANRMP.all = 0xFFFFFFFF;               // Clear all RMPn bits and start
        MessageReceivedCount++;
        //Read from Receive mailboxes and begin checking for data */
                for(j=0; j<32; j++)         // Read & check 16 mailboxes
                {
                   mailbox_read(j);         // This func reads the indicated mailbox data
                   mailbox_check(TestMbox1,TestMbox2,TestMbox3); // Checks the received data
                }
        // all over again...
#else
         ECanaRegs.CANTRS.all = 0xFFFFFFFF;  // Set TRS for all transmit mailboxes
         while(ECanaRegs.CANTA.all != 0xFFFFFFFF ) {}  // Wait for all TAn bits to be set..
         ECanaRegs.CANTA.all = 0xFFFFFFFF;   // Clear all TAn
         MessageSendCount++;
#endif
   /*
        ECanaRegs.CANTRS.all = 0x0000FFFF;  // Set TRS for all transmit mailboxes
       while(ECanaRegs.CANTA.all != 0x0000FFFF ) {}  // Wait for all TAn bits to be set..
       ECanaRegs.CANTA.all = 0x0000FFFF;   // Clear all TAn
       MessageReceivedCount++;

       //Read from Receive mailboxes and begin checking for data
       for(j=16; j<32; j++)         // Read & check 16 mailboxes
       {
          mailbox_read(j);         // This func reads the indicated mailbox data
          mailbox_check(TestMbox1,TestMbox2,TestMbox3); // Checks the received data
       }



        ECanaRegs.CANTRS.all = 0xFFFF0000;  // Set TRS for all transmit mailboxes
        while(ECanaRegs.CANTA.all != 0xFFFF0000 ) {}  // Wait for all TAn bits to be set..
        ECanaRegs.CANTA.all = 0xFFFF0000;   // Clear all TAn
        MessageReceivedCount++;

        //Read from Receive mailboxes and begin checking for data
        for(j=0; j<16; j++)         // Read & check 16 mailboxes
        {
           mailbox_read(j);         // This func reads the indicated mailbox data
           mailbox_check(TestMbox1,TestMbox2,TestMbox3); // Checks the received data
        }

        */

    }
}

// This function reads out the contents of the indicated
// by the Mailbox number (MBXnbr).
void mailbox_read(int16 MBXnbr)
{
   volatile struct MBOX *Mailbox;
   Mailbox = &ECanaMboxes.MBOX0 + MBXnbr;
   TestMbox1 = Mailbox->MDL.all; // = 0x9555AAAn (n is the MBX number)
   TestMbox2 = Mailbox->MDH.all; // = 0x89ABCDEF (a constant)
   TestMbox3 = Mailbox->MSGID.all;// = 0x9555AAAn (n is the MBX number)

} // MSGID of a rcv MBX is transmitted as the MDL data.

void mailbox_check(int32 T1, int32 T2, int32 T3)
{
    if((T1 != T3) || ( T2 != 0x89ABCDEF))
    {
       ErrorCount++;
    }
    else
    {
       PassCount++;
    }
}

//===========================================================================
// No more.
//===========================================================================