Other Parts Discussed in Thread: DRV8312, MOTORWARE, DRV8301, BOOSTXL-DRV8301, INSTASPIN-BLDC, CCSTUDIO, CONTROLSUITE, TMDSCNCD28069ISO, TMDSCNCD28035ISO
We are attempting to run InstaSpin FOC with a Piccolo F28069 card on a DRV8312 Rev D board. The supplied motor works correctly. The test setup is Win7, CCS 5.5, MotorWare 1.0.11 and Piccolo compiler version 6.2.4 as recommended in this forum.
We are trying to get a prototype, ironless, high-speed motor going. It works just fine with hobby ESCs. Both the GUI and the labs have the same characteristics with the new motor. They seem happy identifying the motor (including spinning it at a few hundred rpm during identification) but will not run it at all in the next step of either the GUI or the lab. The identification process also comes up with numbers that can be an order of magnitude different from run to run.
The numbers they it comes up with in either the GUI or the labs are similar and random:
Rs .11 (That is about right. I have sen it come up with everything from 8e-6 to 5 ohms)
Ld Who knows? It has come up with anything from 4.9e-10 to .0006
Lq Who knows? It has come up with anything 4.9e-10 to .0006
Flux .118 is most common though it has gotten as low as .035
I am at a loss as to how to proceed and would greatly appreciate your help.
Thank you,
Norm Dawley