Other Parts Discussed in Thread: TMS320F28335, AM26LV32, SN65HVD30, DS8921
Hello,
I need to measure the rotor position and speed from an induction motor for my Master Thesis about DFIG's.
I have an eZdsp F28335 development board from Spectrum Digital and I have found that there is an eQEP module on the TMS320F28335 microcontroller in order to interface an incremental position encoder.
Now I am searching the incremental position encoder. Most commonly used output signals are Push Pull, RS422 and open collector.
Which one is supported by the eQEP-module?
Which method is preferred?
Is it possible to directly connect the outputs from the incremental encoder(A, B, Index) to the inputs of the eZdsp (EQEPxA, EQEPxB, EQEPxI)?
Thanks in Advance!
Pieter Gervoyse,
Master Student at the KU Leuven, Belgium