Hi All:
I am now trying to do flash programming through CKFA
and my project include CLA application,
My function works will but the CLA application ,
for example,I designed an procedure that send a value to my MCU through CAN BUS ,
and transmit to CLA module to calculate a new value then send it back
I can send through CAN BUS ,but it returns a constant value which is not correct
the linker file I used in CKFA program and my application program is attached here,
I don't know if I do any thing wrong so the CLA application doesn't work normally
Thanks for your reading!
Regards
Will
http://e2e.ti.com/cfs-file.ashx/__key/communityserver-discussions-components-files/171/2248.linker_5F00_files-.7z