Hi all.
When the "PIE VECTOR ADDRESS MISMATCH" function of Concerto occurs,
can I be the Low output PWM of Concerto?
As Trip Zone function.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Yes when "PIE VECTOR ADDRESS MISMATCH" happens, this error (PIEERR) is fed to ePWM as one of the TRIP input (TRIPIN15) to trip the ePWM output.
Regards,
Vivek Singh