I am just beginning to learn DSP 28335 with a Programming Board. I can run the example code for the first time and it works quite well. But when I want to run the second example, I have to shut down the power supply of the board and unplug the USB. Then restart the board for the second example.
It is working quite well at the moment, however I think it is a bit tedious as I have to restart the board for each debugging. I am wondering how can I debug the example without so many plugging the emulator USB and the power supply. Thanks.