This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28377D SPI FIFO Level

SPI Feature

16-level transmit / receive FIFO (SPRUHM8 page 1930)

Transmit FIFO has 4 words, which is the maximum (SPRUHM8 page 1968)

Receive FIFO has 4 words, which is the maximum (SPRUHM8 page 1970)

What is the true?