This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem when build file .out CCSv5.5 for card TMS320F28335



Hi,

When I build from Simulink to .out file (for load to CCSv5.5 card F28335) it has errors:

<Linking>
"C:\Users\NGOCSA~1\AppData\Local\Temp\006123", line 26: error: cannot
find file "S:/Program\
"
"C:\Users\NGOCSA~1\AppData\Local\Temp\006123", line 27: error: cannot
find file
"Files/MATLAB/R2013a/toolbox/idelink/extensions/ticcs/rtlib/IQmath_fpu32.lib
"
error: errors encountered during linking; "./CustomMW/pulse.out" not built

>> Compilation failure
gmake: *** [CustomMW/pulse.out] Error 1

I have run checkEnvSetup('ccsv5','F28335','check') and xmakefilesetupeverything is normally.

I don't know what is this error and how to solve it? 

Furthermore, in other computer I build successfully and load to CCSv5.5 to run the card, make PWM pulse. However, the PWM output frequency I set in PWM Generator block is 10kHz, but the oscilloscope show that it's only 330Hz ?! 

Is there any suggestion for me? Thank you!