This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HVPSFB PCMC epwm2 slave timing waveforms

Hello, I'm wondering about the slave configuration of ePWM2 in the HVPSFB PCMC.  I see that the TBPRD of ePWM2 is set to 299 and is upcount only.  I realize that ePWM1 TBPRD is set to 300 and generates a sync pulse for ePWM2 at TBCTR = TBCMPB = 0 & TBCTR=TBCMPB = 300.  I noticed in HVPSFB-DPL-ISR.asm that the A&B outputs of ePWM2 action qualifier block are setup to not take any action if ePWM2.TBCTR = ZRO.  My question is are there intervals in which ePWM2.TBCTR doesn't reach the PRD.  Thanks.