Hello,
I damaged PR798.
I think I destroyed a resistor or capacitor which is on bottom. But I cannot remove it from HVPSFB kit.
Does anybody have advice?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kazim,
Removing these modules is a bit tricky but it is doable. I am sympathetic as I have done this job several times.
You'll need to desolder the individual pins with a soldering iron that has a pretty large tip and then use solder wick to soak up the solder. The key is to make sure that the solder liquifies.
Occasionally, you may desolder a pin, realize that it's not removed adequately, need to resolder it, and then re-desolder it. Go one at a time through the pins and you'll eventually get it off.
Note that if you destroyed a capacitor (and especially a resistor) you likely damaged more than just the one component. Once you get the PR798 off I would recommend checking for shorts between powers and grounds, etc.
Thank you,
Brett