I am using an boostxl- drv8301 kit with a motor identified with instaspin with 8 pairs of poles, Rs 2.3 ohms, Ld, Lq = 0.220 mH, 24 V and works fine in one rotation direction , but not in the reverse direction. If the SPEEDREF is negative, the motor stops. It can be due to incorrect motor parameters , speed pid values?