Other Parts Discussed in Thread: MOTORWARE
Hello Chris,
Wishing to use FAST without CTRL. Having some trouble figuring out which elements of which structures are actually needed by FAST alone and which are not. And how to actually drive FAST, among other reasons because in its state machine some transitions seem to be triggered by inputs from CTRL.
It seems some elements required by FAST and CTRL are mixed up in some structures maybe. Some CTRL actions may effect EST or not.
Do you have or could you generate a simple list of structures and indicate those elements within those strutures that are required by FAST. And what would be the required sequence of setup , EST enable, disable, init, run, resetcounter, idle etc. by EST in a minumum situation of just getting it to run the rotor flux angle estimator.??
Would also be good if the same could be done for the FAST motor ID but I think you have already indicated we are hanging out to dry on that one!
Yes I could derive this by persuing your code (eventually) and stepping through your code (though I have none of your hardware) and a little or a lot of trial and error and fiddling. That is a very ineffective way of proceeding.
Hoping for a positive response.
Roger