Hello,
In lab5c, to ID the inertia, we attach the system to the motor, but free of load. (Ex: attach drum but no clothes, no water, in washing machine). Then, I'm wondering, to ID the motor parameters, is the lab2a should be same case?? Or, we should remove all the attachment from the shaft, leaving the motor itself alone??