Other Parts Discussed in Thread: TMS320F28069
Good day,
I am working with the control card tms320f28069 of the DRV8301-69M kit for a control of a motor. This motor operated well until yesterday, and i try to operate again today and the motor don't run again.
for this reason i try to turn on again the card but it card have a hottest temperature or it overheats and don't permit connect the F2806x ISO controlCARD (the smaller), with the DVR8301-69M card (the big card).
other problem that i have is that it do not allow conect with the PC and with the source of the card, and my motor don't work any more.
I have a real problem because i don't know how i can review the card and i don't know how it will can be repaired. ¿What are the terms of the Waranty or how much is the cost of the reparation?.
And i need operate again with this card. Thanks for your fast answer and for your support.