Dear TI Team,
for the Concerto (F28M36) I need to setup an single PWM channel which is able to send out a predefined (e.g. 16)
number of pulses on request only.
After the output of these predefined number of PWM pulses, the PWM channel should stop autonomous
without using an external TZ signal or furthermore controlling.
e.g.:
Start of PWM pulses autonom PWM stop
v v
|-| |-| |-| |-| |-| |-| |-| |-|
------------| |---| |---| |---| |---| |---| |---| |---| |--------------
Is there any code sample or can you give me a hint to realize it?
Thanks
WJ