Hi all,
I am using the C2000 launchpad and have a working ADC code, however I would like to refine and need to be sure I am interpreting the actions correctly. I have been reading the ADC and comparator application note spruge5f.pdf. I have some bits of my code below to illustrate my setup.
The ADC is triggered by the ePWM, which is running at 15kHz, I have the following PWM functions enabled:
// Enables the pulse width modulation (PWM) start of conversion (SOC) A pulse generation
PWM_enableSocAPulse(myPwm1);
// Enables the pulse width modulation (PWM) start of conversion (SOC) A pulse generation
PWM_setSocAPulseSrc(myPwm1, PWM_SocPulseSrc_CounterEqualCmpAIncr);
// Sets the pulse width modulation (PWM) start of conversion (SOC) A interrupt period
PWM_setSocAPeriod(myPwm1, PWM_SocPeriod_SecondEvent);
The ADC code is then setup as follows, I use all 16 Soc's but not added them all here just to keep the code shorter:
void init_ADC(void)
{
// Enables the ADC band gap circuit
ADC_enableBandGap(myAdc);
// Enables the ADC reference buffers circuit
ADC_enableRefBuffers(myAdc);
// Powers up the ADC
ADC_powerUp(myAdc);
// Enables the ADC
ADC_enable(myAdc);
// Sets the voltage reference source
ADC_setVoltRefSrc(myAdc, ADC_VoltageRefSrc_Int);
// Clear ADCINT1 flag reinitialize for next SOC
ADC_clearIntFlag(myAdc, ADC_IntNumber_1);
// Enables the specified ADC interrupt
PIE_enableAdcInt(myPie, ADC_IntNumber_1);
// Enables the ADC interrupt
ADC_enableInt(myAdc, ADC_IntNumber_1);
// Sets the interrupt pulse generation mode
ADC_setIntPulseGenMode(myAdc, ADC_IntPulseGenMode_Prior); //ADCINT1 trips after AdcResults latch
// Enables ADC interrupt
ADC_enableInt(myAdc, ADC_IntNumber_1);
// Sets the interrupt mode
ADC_setIntMode(myAdc, ADC_IntNumber_1, ADC_IntMode_ClearFlag); // Disable ADCINT1 Continuous mode
// Sets the interrupt source
ADC_setIntSrc(myAdc, ADC_IntNumber_1, ADC_IntSrc_EOC15); // Setup EOC15 (all 16 soc's used) to trigger ADCINT1
// Sets the start-of-conversion (SOC) channel number
ADC_setSocChanNumber (myAdc, ADC_SocNumber_0, ADC_SocChanNumber_A0);
ADC_setSocChanNumber (myAdc, ADC_SocNumber_1, ADC_SocChanNumber_A1);
ADC_setSocChanNumber (myAdc, ADC_SocNumber_2, ADC_SocChanNumber_A2);
// Sets the start-of-conversion (SOC) trigger source
ADC_setSocTrigSrc(myAdc, ADC_SocNumber_0, ADC_SocTrigSrc_EPWM1_ADCSOCA);
ADC_setSocTrigSrc(myAdc, ADC_SocNumber_1, ADC_SocTrigSrc_EPWM1_ADCSOCA);
ADC_setSocTrigSrc(myAdc, ADC_SocNumber_2, ADC_SocTrigSrc_EPWM1_ADCSOCA);
// Sets the start-of-conversion (SOC) sample delay
ADC_setSocSampleWindow(myAdc, ADC_SocNumber_0, ADC_SocSampleWindow_20_cycles);
ADC_setSocSampleWindow(myAdc, ADC_SocNumber_1, ADC_SocSampleWindow_20_cycles);
ADC_setSocSampleWindow(myAdc, ADC_SocNumber_2, ADC_SocSampleWindow_20_cycles);
}
Then I read the ADC buffers with the following code, and my question mainly involves this, but the way I have it setup is relevant so included for completeness:
while(AdcRegs.ADCINTFLG.bit.ADCINT1 == 0){} // Wait until ADCINT1 is tripped ADC_getIntStatus(myAdc, ADC_IntNumber_1);
//Voltage1[ConversionCount] = ADC_readResult(myAdc, ADC_ResultNumber_1);
//Voltage2[ConversionCount] = ADC_readResult(myAdc, ADC_ResultNumber_2);
ADC0 = AdcResult.ADCRESULT0; // Input Volts - First of 1st sample block
ADC1 = AdcResult.ADCRESULT1; // Input Current -
ADC2 = AdcResult.ADCRESULT2; // Output Volts -
ADC3 = AdcResult.ADCRESULT3; // Output Current - Last of 1st sample block
ADC4 = AdcResult.ADCRESULT4; // Input Volts - First of 2nd sample block
ADC5 = AdcResult.ADCRESULT5; // Input Current -
ADC6 = AdcResult.ADCRESULT6; // Output Volts -
ADC7 = AdcResult.ADCRESULT7; // Output Current - Last of 2nd sample block
ADC8 = AdcResult.ADCRESULT8; // Input Volts - First of 3rd sample block
ADC9 = AdcResult.ADCRESULT9; // Input Current -
ADC10 = AdcResult.ADCRESULT10; // Output Volts -
ADC11 = AdcResult.ADCRESULT11; // Output Current - Last of 3rd sample block
ADC12 = AdcResult.ADCRESULT12; // Input Volts - First of 4th sample block
ADC13 = AdcResult.ADCRESULT13; // Input Current -
ADC14 = AdcResult.ADCRESULT14; // Output Volts -
ADC15 = AdcResult.ADCRESULT15; // Output Current - Last of 4th sample block
// Clear ADCINT1 flag reinitialize for next SOC
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; // Clear ADCINT1 ADC_clearIntFlag(myAdc, ADC_IntNumber_1);
Ok, so my understanding is that the ePWM will trigger a the ADC to capture at 15kHz. I could set my code to read the ADC buffers at 40kHz, but it would still only read the data from the ADC buffer at 15kHz as my code would be waiting for the line of code below
while(AdcRegs.ADCINTFLG.bit.ADCINT1 == 0){}
and then it would clear this flag and repeat the cycle with the line of code below
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
I am pretty sure that is right but if not can someone put me straight?
Cheers,
Ant