This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M36 ePWM Chn-8

Dear TI Team,

for the Concerto (F28M36 Concerto Control Card) we need PWM channel 1 through 8.

For the PWM channel 1 through 7, the setup and initialization can be done. No issues.

However for the PWM channel 8 (and 9) the setup and initialization can NOT be done.
All setups on the M3 side are done.
Even via the 'CCS-Register-Window' in debugging mode, the setup of PWM channel 8 (and 9)
is not possible. All (writeable) ePWM registers are always ZERO.

Is there any restriction for the PWM channel 8 (and 9) or what has to be done to use PWM channel 8 (and 9)?


Thanks
WJ