Other Parts Discussed in Thread: DRV8301, BOOSTXL-DRV8301, MOTORWARE
Where in the Instaspin libraries is the DRV8301 shunt amplifier gain configured? I am experimenting with a new board which uses pretty much the same schematic as the BOOSTXL-DRV8301 but with components spec'd similarly to the DRV8301 High Current EVM. Just to test this out I'm running lab 2c on it but I need to change the amplifier gain to 20. Also, I am seeing massively erroneous Rs_ohm estimates (~2e+08) which may be because I haven't adjusted programmable gains yet while the external amplifier has a fixed gain. I am attaching my user.h file in case it becomes useful. I have only changed the voltage and current scaling - otherwise this is the same file I used to successfully identify this motor using the BOOSTXL-DRV8301. Thanks in advance.