Other Parts Discussed in Thread: TMS320F2808
Hi,
I'm using the dead-band module in the processor, TMS320F2808 for controlling IGBTs on the same leg of an H-bridge Inverter. I have a question about the minimum pulse-width that can be supported by the dead-band module.
My RED and FED counters are set to 260 (which corresponds to a delay of 2.6 usecs). If the pulse width of the control is 1 usecs, I observe that the dead-band module totally turns OFF the PWM Output. When I comment out the dead-band module code, I'm able to see the 1 usecs pulse at the PWM Output. However, when I turn back on the dead-band module, I do not see the pulses... Here's the configuration of the dead-band module that I'm using...
EPwm1Regs.TBPRD = HZ50_DOWN_COUNT; // Time base = 2*TIMER_PRD = 0x9c4
EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm1Regs.TBCTR = 0x0000; // Clear counter
// Setup TBCLK
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_DOWN; // Symmetrical mode
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading - Master module
EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE; // Sync Down-stream module
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // High Speed Clock ratio is unity
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1; // Sysclock ratio is unity
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on CTR = Zero
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // Load on CTR = Zero
// Setup compare
EPwm1Regs.CMPA.half.CMPA = KHZ20_COUNT_TIMER_PRD >> 1;
EPwm1Regs.CMPB = KHZ20_COUNT_TIMER_PRD >> 1;
// down counter
EPwm1Regs.AQCTLA.bit.ZRO = AQ_CLEAR;
EPwm1Regs.AQCTLA.bit.CAD = AQ_SET;
EPwm1Regs.AQCTLB.bit.ZRO = AQ_SET;
EPwm1Regs.AQCTLB.bit.CAD = AQ_CLEAR;
// Enable Dead-band module
EPwm1Regs.DBCTL.bit.IN_MODE = DBA_ALL;
EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm1Regs.DBFED = 260;
EPwm1Regs.DBRED = 260;
Any help in this regard is highly appreciated !!!
Vishal