Other Parts Discussed in Thread: DRV8312, DRV8301, BOOSTXL-DRV8301
Hi,
Some questions about sensors when designing my own HW.
The goal of the system is to run at max speed and do field weakening (i.e modulation index > 1).
For the above purpose, I thought about the following configuration:
1. Voltage sensors - Do the voltage dividing with the resistors, then in order to match better the impedance with the ADC, I thought about using op-amps with 50 Ohm resistor at the output (from TI of course) and realize the first order filter on the op-amp.
2. Current sensor - in order not to get into trouble when modulation index>1, I thought of using current sensors directly on the phase (LEM etc). Then the question is when to sample. I thought to configure the PWM for SOC when CTR=PRD. If doing so, do I still need to run the "ignoreShunt","SVM reconstruction" etc various functions ?
3. Wire and configure the ADC channels to use both S/H circuits. If doing so, I think the "NonOverLap" bit needs to be set..
What do you think ?
Is that the right configuration for running at modulation index > 1 ?
thanks a lot