Other Parts Discussed in Thread: CONTROLSUITE
Hello,
Working with F28377D (on a TMDXDOCK28377D board), using CCSv6-beta 4,
I need to switch execution from 1st FLASH program to a 2nd program FLASH, on same CPU.
Can I have some example/guidelines to do the following:
---------------------------------------------------------------------------
1. How can I burn two programs to a FLASH of the same CPU, CPU1?
2. How can I decide which of the two program to execute after F28377D is reset & booted?
3. How can I switch execution from 1st FLASH program to the 2nd FLASH program (&then back from 2nd to 1st)?
Thanks
Roni