Other Parts Discussed in Thread: TMS320F28027, CONTROLSUITE
Hi all,
For a final course project I am going to attempt to build a basic PFC using the TMS320F28027 Launchpad, I am at the stage of just over viewing, and deciding how to implement. I need to feed three signals back to the ADC, 2 of these should not be an issue, however for the 3rd I am struggling how to sample and get the information I need.
The third signal will be a sample of a rectified AC (~50HZ), the rectified AC will not be smoothed so it will appear to be double the frequency. This method for counting is referenced in a few PFC documents I have read, and the maths behind it seems fairly simple. I have enclosed an extract below from the spra902a.pdf
2 things need to be extracted from the sampled rectified signal, the frequency and also the average voltage. The average voltage is fairly straightforward as just requires samples, but the counting part I am struggling with at the moment!
I am not after code just some pointers and ideas how I might approach this issue with the C2000, and best practice. I have made a frequency counter before using the LM3S but this was fed with square waves so easy to count edge triggers.
Thanks,
Ant