Other Parts Discussed in Thread: CONTROLSUITE, MOTORWARE, TMDSHVMTRINSPIN, CCSTUDIO
Hi, I've read lots and lots of great material here and in manuals, bought a kit, spun the proto-motor in the labs, and now that it is time to start custom design, a few questions arose. Background: I am in charge of motor control for a high-end consumer product (tool). The Piccolo series looks like a great match. These questions are so simple that perhaps I've missed the answers, or your development team thought them obvious! Nonetheless:
1. How do I create a development setup that allows TI updates when desired, yet may also be frozen? For instance, in CCS one may create a new workspace, or a new project. There seem to be enough gotchas, that it seems best to start with a lab and modify (or not?).
2. The many tools confuse me, as there seems to be overlap. I started with the eval kit CD, but went on to update CCS, Motorware, ControlSuite (but not the RTOS, was it included?). These questions are related:
A. Are these packages independent?
B. Can you give a basic rundown and contrast for each? I read up on them, but, for instance, ControlSuite calls itself "a comprehensive suite of software for C2000 microcontrollers," but the word "comprehensive" seems a little over-reaching.
C. The ControlSuite guide, SPRUGU2B, is nearly 3 years old and doesn't mention support for TMDSHVMTRINSPIN, though it seemed to be in the download.
Thanks, as always. My motor selection is coming close and the drive design path is nearly due!