Other Parts Discussed in Thread: MOTORWARE
Hello e2e community,
I m using the drv8301-69M-KIT in light weight electric cart (nearly 100 kilograms without the driver) and i just entered the Instaspin-MOTION labs.
I went through the labs 2-4 with no problem and i decided to go to lab 5c in order to finally tune the motor in the next two projects. To my understanding, in order to do the inertia identification the motor should be connected to the wheel (it gives power to one wheel through a gear) while the cart isn't on the ground so the wheel is free to rotate. When the procedure started (Flag_Run_Identify set to 1) the wheel did not rotate and a high pitch sound was produced by the motor. I changed the StopSpeedRed_krmp, VellGoaldSpeed_krpm, VellidTorqueRampTime_sec by the problem insisted.
Finally i stopped my experiments because i was afraid i would damage the motor. I attach the user.h file and i m free for suggestions!
Best Regards,
Alexandros