This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2803x Master to 2802x Slave SPI communication

I'm attempting to transmit data from a 28034 to one of 4 slave 28027s through SPI, but by slightly altering the SPI Loopback example code, I have not been able to accomplish this.  I've flashed the 28034 and have a scope on it.  I can see that the signal I'm sending from the master is reaching the SOMI pins on each of the slave 28027s, but I haven't been able to actually receive the signal while debugging on any of the 28027s.

Here are the files I'm using for my 28027:

// TI File $Revision: /main/4 $
// Checkin $Date: October 6, 2010   14:43:16 $
//###########################################################################
//
// FILE:   Example_2802xSpi_FFDLB.c
//
// TITLE:  DSP2802x Device Spi Digital Loop Back program.
//
// ASSUMPTIONS:
//
//    This program requires the DSP2802x header files.
//
//    This program uses the internal loop back test mode of the peripheral.
//    Other then boot mode pin configuration, no other hardware configuration
//    is required.
//
//    As supplied, this project is configured for "boot to SARAM"
//    operation.  The 2802x Boot Mode table is shown below.
//    For information on configuring the boot mode of an eZdsp,
//    please refer to the documentation included with the eZdsp,
//
//    $Boot_Table
//    While an emulator is connected to your device, the TRSTn pin = 1,
//    which sets the device into EMU_BOOT boot mode. In this mode, the
//    peripheral boot modes are as follows:
//
//      Boot Mode:   EMU_KEY        EMU_BMODE
//                   (0xD00)	     (0xD01)
//      ---------------------------------------
//      Wait		 !=0x55AA        X
//      I/O		     0x55AA	         0x0000
//      SCI		     0x55AA	         0x0001
//      Wait 	     0x55AA	         0x0002
//      Get_Mode	 0x55AA	         0x0003
//      SPI		     0x55AA	         0x0004
//      I2C		     0x55AA	         0x0005
//      OTP		     0x55AA	         0x0006
//      Wait		 0x55AA	         0x0007
//      Wait		 0x55AA	         0x0008
//      SARAM		 0x55AA	         0x000A	  <-- "Boot to SARAM"
//      Flash		 0x55AA	         0x000B
//	    Wait		 0x55AA          Other
//
//   Write EMU_KEY to 0xD00 and EMU_BMODE to 0xD01 via the debugger
//   according to the Boot Mode Table above. Build/Load project,
//   Reset the device, and Run example
//
//   $End_Boot_Table
//
// DESCRIPTION:
//
//    This program is a SPI example that uses the internal loopback of
//    the peripheral.  Interrupts are not used.
//
//    A stream of data is sent and then compared to the recieved stream.
//
//    The sent data looks like this:
//    0000 0001 0002 0003 0004 0005 0006 0007 .... FFFE FFFF
//
//    This pattern is repeated forever.
//
//          Watch Variables:
//                sdata - sent data
//                rdata - received data
//
////###########################################################################
// Original Author: S.S.
//
// $TI Release: 2802x C/C++ Header Files and Peripheral Examples V1.28 $
// $Release Date: October 15, 2010 $
//###########################################################################

#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

// Prototype statements for functions found within this file.
// interrupt void ISRTimer2(void);
void delay_loop(void);
void spi_xmit(Uint16 a);
void spi_fifo_init(void);
void spi_init(void);
void error(void);

void main(void)
{
   Uint16 sdata;  // send data
   Uint16 rdata;  // received data

// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2802x_SysCtrl.c file.
   InitSysCtrl();

// Step 2. Initalize GPIO:
// This example function is found in the DSP2802x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio();  // Skipped for this example
// Setup only the GP I/O only for SPI-A functionality
// This function is found in DSP2802x_Spi.c
   InitSpiaGpio();

// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
   DINT;

// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2802x_PieCtrl.c file.
   InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
   IER = 0x0000;
   IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in DSP2802x_DefaultIsr.c.
// This function is found in DSP2802x_PieVect.c.
   InitPieVectTable();

// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2802x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
   spi_fifo_init();	  // Initialize the Spi FIFO
   spi_init();		  // init SPI

// Step 5. User specific code:
// Interrupts are not used in this example.
   sdata = 0x0000;
   for(;;)
   {
	   /*
	    * 2802x processors are slaves, so they will just receive data
	    */
	   // Wait until data is received

	   while(SpiaRegs.SPIFFRX.bit.RXFFST !=1) { }
	   rdata = SpiaRegs.SPIRXBUF;
	   if (rdata == 0x00AA)
	   {
		   spi_xmit(0x000A);
	   }
   }
}

// Step 7. Insert all local Interrupt Service Routines (ISRs) and functions here:

void delay_loop()
{
    long      i;
    for (i = 0; i < 1000000; i++) {}
}

void error(void)
{
    asm("     ESTOP0");						// Test failed!! Stop!
    for (;;);
}

void spi_init()
{
	SpiaRegs.SPICCR.all =0x000F;	             // Reset on, rising edge, 16-bit char bits
	SpiaRegs.SPICTL.all =0x0006;    		     // Enable master mode, normal phase,
                                                 // enable talk, and SPI int disabled.
	SpiaRegs.SPICTL.bit.SPIINTENA = 1;
	SpiaRegs.SPICTL.bit.MASTER_SLAVE = 0;		 // Changing it to slave
	SpiaRegs.SPIBRR =0x007F;
    SpiaRegs.SPICCR.all =0x009F;		         // Relinquish SPI from Reset
    SpiaRegs.SPIPRI.bit.FREE = 1;                // Set so breakpoints don't disturb xmission
}

void spi_xmit(Uint16 a)
{
    SpiaRegs.SPITXBUF=a;
}

void spi_fifo_init()
{
// Initialize SPI FIFO registers
    SpiaRegs.SPIFFTX.all=0xE040;
    SpiaRegs.SPIFFRX.all=0x2044;
    SpiaRegs.SPIFFCT.all=0x0;
}

//===========================================================================
// No more.
//===========================================================================

 

And

// TI File $Revision: /main/1 $
// Checkin $Date: August 14, 2008   16:58:49 $
//###########################################################################
//
// FILE:   DSP2802x_Spi.c
//
// TITLE:  DSP2802x SPI Initialization & Support Functions.
//
//###########################################################################
// $TI Release: 2802x C/C++ Header Files and Peripheral Examples V1.28 $
// $Release Date: October 15, 2010 $
//###########################################################################

#include "DSP2802x_Device.h"     // DSP2802x Headerfile Include File
#include "DSP2802x_Examples.h"   // DSP2802x Examples Include File

//---------------------------------------------------------------------------
// InitSPI:
//---------------------------------------------------------------------------
// This function initializes the SPI(s) to a known state.
//
void InitSpi(void)
{
   // Initialize SPI-A

   //tbd...

}

//---------------------------------------------------------------------------
// Example: InitSpiGpio:
//---------------------------------------------------------------------------
// This function initializes GPIO pins to function as SPI pins
//
// Each GPIO pin can be configured as a GPIO pin or up to 3 different
// peripheral functional pins. By default all pins come up as GPIO
// inputs after reset.
//
// Caution:
// For each SPI peripheral
// Only one GPIO pin should be enabled for SPISOMO operation.
// Only one GPIO pin should be enabled for SPISOMI operation.
// Only one GPIO pin should be enabled for SPICLKA operation.
// Only one GPIO pin should be enabled for SPISTEA operation.
// Comment out other unwanted lines.

void InitSpiGpio()
{

   InitSpiaGpio();
}

void InitSpiaGpio()
{

   EALLOW;

/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAPUD.bit.GPIO16 = 0;   // Enable pull-up on GPIO16 (SPISIMOA)
    GpioCtrlRegs.GPAPUD.bit.GPIO17 = 0;   // Enable pull-up on GPIO17 (SPISOMIA)
    GpioCtrlRegs.GPAPUD.bit.GPIO18 = 0;   // Enable pull-up on GPIO18 (SPICLKA)
    GpioCtrlRegs.GPAPUD.bit.GPIO19 = 0;   // Enable pull-up on GPIO19 (SPISTEA)

/* Set qualification for selected pins to asynch only */
// This will select asynch (no qualification) for the selected pins.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAQSEL2.bit.GPIO16 = 3; // Asynch input GPIO16 (SPISIMOA)
    GpioCtrlRegs.GPAQSEL2.bit.GPIO17 = 3; // Asynch input GPIO17 (SPISOMIA)
    GpioCtrlRegs.GPAQSEL2.bit.GPIO18 = 3; // Asynch input GPIO18 (SPICLKA)
    GpioCtrlRegs.GPAQSEL2.bit.GPIO19 = 3; // Asynch input GPIO19 (SPISTEA)

/* Configure SPI-A pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be SPI functional pins.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAMUX2.bit.GPIO16 = 1; // Configure GPIO16 as SPISIMOA
    GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 1; // Configure GPIO17 as SPISOMIA
    GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 1; // Configure GPIO18 as SPICLKA
    GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 1; // Configure GPIO19 as SPISTEA

    EDIS;
}

//===========================================================================
// End of file.
//===========================================================================

The ones for my Master 28034:

//###########################################################################
// Description:
//! \addtogroup f2803x_example_list
//! <h1>ePWM Timer Interrupt From Flash (flash_f28035)</h1>
//!
//! This example runs the ePWM interrupt example from flash. ePwm1 Interrupt 
//! will run from RAM and puts the flash into sleep mode. ePwm2 Interrupt 
//! will run from RAM and puts the flash into standby mode. ePWM3 Interrupt
//! will run from FLASH. All timers have the same period. The timers are 
//! started sync'ed. An interrupt is taken on a zero event for each ePWM 
//! timer.GPIO34 is toggled while in the background loop.
//! Note:
//!   - ePWM1: takes an interrupt every event
//!   - ePWM2: takes an interrupt every 2nd event
//!   - ePWM3: takes an interrupt every 3rd event 
//! Thus the Interrupt count for ePWM1, ePWM4-ePWM6 should be equal
//! The interrupt count for ePWM2 should be about half that of ePWM1
//! and the interrupt count for ePWM3 should be about 1/3 that of ePWM1
//! 
//! Follow these steps to run the program.
//!   - Build the project
//!   - Flash the .out file into the device.
//!   - Set the hardware jumpers to boot to Flash (put position 1 and 2 of 
//!     SW2 on control Card to ON position).
//!   - Use the included GEL file to load the project, symbols
//!     defined within the project and the variables into the watch
//!     window.
//! 
//! Steps that were taken to convert the ePWM example from RAM
//! to Flash execution: 
//! - Change the linker cmd file to reflect the flash memory map.
//! - Make sure any initialized sections are mapped to Flash.
//!   In SDFlash utility this can be checked by the View->Coff/Hex
//!   status utility. Any section marked as "load" should be
//!   allocated to Flash.
//! - Make sure there is a branch instruction from the entry to Flash
//!   at 0x3F7FF6 to the beginning of code execution. This example
//!   uses the DSP0x_CodeStartBranch.asm file to accomplish this.
//! - Set boot mode Jumpers to "boot to Flash"
//! - For best performance from the flash, modify the waitstates
//!   and enable the flash pipeline as shown in this example.
//!   Note: any code that manipulates the flash waitstate and pipeline
//!   control must be run from RAM. Thus these functions are located
//!   in their own memory section called ramfuncs.
//! 
//! \b Watch \b Variables \n
//!  - EPwm1TimerIntCount
//!  - EPwm2TimerIntCount
//!  - EPwm3TimerIntCount
//
//###########################################################################
// $TI Release: F2803x C/C++ Header Files and Peripheral Examples V127 $
// $Release Date: March 30, 2013 $
//###########################################################################

#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File
#include <string.h>
#include <stdint.h>

// Prototype statements for functions found within this file.
void spi_xmit(Uint16 a);
void spi_fifo_init(void);
void spi_init(void);
void error(void);

// Configure which ePWM timer interrupts are enabled at the PIE level:
// 1 = enabled,  0 = disabled
#define PWM1_INT_ENABLE  1
#define PWM2_INT_ENABLE  1
#define PWM3_INT_ENABLE  1

// Configure the period for each timer
#define PWM1_TIMER_TBPRD   0x1FFF
#define PWM2_TIMER_TBPRD   0x1FFF
#define PWM3_TIMER_TBPRD   0x1FFF

// Make this long enough so that we can see an LED toggle
#define DELAY 1000000L

// Functions that will be run from RAM need to be assigned to
// a different section.  This section will then be mapped using
// the linker cmd file.
#pragma CODE_SECTION(epwm1_timer_isr, "ramfuncs");
#pragma CODE_SECTION(epwm2_timer_isr, "ramfuncs");

// Prototype statements for functions found within this file.
__interrupt void epwm1_timer_isr(void);
__interrupt void epwm2_timer_isr(void);
__interrupt void epwm3_timer_isr(void);
void InitEPwmTimer(void);

// Global variables used in this example
Uint32  EPwm1TimerIntCount;
Uint32  EPwm2TimerIntCount;
Uint32  EPwm3TimerIntCount;
Uint32  LoopCount;

// These are defined by the linker (see F2808.cmd)
extern Uint16 RamfuncsLoadStart;
extern Uint16 RamfuncsLoadSize;
extern Uint16 RamfuncsRunStart;

void main(void)
{
	Uint16 sdata;  // send data
	Uint16 rdata;  // received data

// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2803x_SysCtrl.c file.
   InitSysCtrl();

// Step 2. Initalize GPIO:
// This example function is found in the DSP2803x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio();  // Skipped for this example
   InitSpiaGpio();
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
   DINT;

// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2803x_PieCtrl.c file.
   InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
   IER = 0x0000;
   IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in DSP2803x_DefaultIsr.c.
// This function is found in DSP2803x_PieVect.c.
   InitPieVectTable();

// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
   EALLOW;  // This is needed to write to EALLOW protected registers
   PieVectTable.EPWM1_INT = &epwm1_timer_isr;
   PieVectTable.EPWM2_INT = &epwm2_timer_isr;
   PieVectTable.EPWM3_INT = &epwm3_timer_isr;
   EDIS;    // This is needed to disable write to EALLOW protected registers

// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2803x_InitPeripherals.c
// InitPeripherals();  // Not required for this example
   InitEPwmTimer();    // For this example, only initialize the ePWM Timers

// Step 5. User specific code, enable interrupts:

// Copy time critical code and Flash setup code to RAM
// This includes the following ISR functions: epwm1_timer_isr(), epwm2_timer_isr()
// epwm3_timer_isr and and InitFlash();
// The  RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart
// symbols are created by the linker. Refer to the F2808.cmd file.
   memcpy((uint16_t *)&RamfuncsRunStart,(uint16_t *)&RamfuncsLoadStart, (unsigned long)&RamfuncsLoadSize);

// Call Flash Initialization to setup flash waitstates
// This function must reside in RAM
   InitFlash();

// Initalize counters:
   EPwm1TimerIntCount = 0;
   EPwm2TimerIntCount = 0;
   EPwm3TimerIntCount = 0;
   LoopCount = 0;

// Enable CPU INT3 which is connected to EPWM1-3 INT:
   IER |= M_INT3;

// Enable EPWM INTn in the PIE: Group 3 interrupt 1-3
   PieCtrlRegs.PIEIER3.bit.INTx1 = PWM1_INT_ENABLE;
   PieCtrlRegs.PIEIER3.bit.INTx2 = PWM2_INT_ENABLE;
   PieCtrlRegs.PIEIER3.bit.INTx3 = PWM3_INT_ENABLE;

// Enable global Interrupts and higher priority real-time debug events:
   EINT;   // Enable Global interrupt INTM
   ERTM;   // Enable Global realtime interrupt DBGM

// Step 6. IDLE loop. Just sit and loop forever (optional):
   EALLOW;
   GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0;
   GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;
   EDIS;

   // Step 4. Initialize all the Device Peripherals:
   // This function is found in DSP2803x_InitPeripherals.c
   // InitPeripherals(); // Not required for this example
      spi_fifo_init();	  // Initialize the Spi FIFO
      spi_init();		  // init SPI

   // Step 5. User specific code:
   // Interrupts are not used in this example.
      sdata = 0x00AA;
      for(;;)
      {
   		/*
   		* 2803x is the Master, master will just transmit data
   		*/
   	   // Transmit data
   	   spi_xmit(sdata);
   	   //sdata++;
      }

}


void error(void)
{
    __asm("     ESTOP0");						// Test failed!! Stop!
    for (;;);
}

void spi_init()
{
	SpiaRegs.SPICCR.all =0x000F;	             // Reset on, rising edge, 16-bit char bits
	SpiaRegs.SPICTL.all =0x0006;    		     // Enable master mode, normal phase,
                                                 // enable talk, and SPI int disabled.
	SpiaRegs.SPICTL.bit.MASTER_SLAVE = 1;		// Set to master
	SpiaRegs.SPIBRR =0x007F;
    SpiaRegs.SPICCR.all =0x009F;		         // Relinquish SPI from Reset
    SpiaRegs.SPIPRI.bit.FREE = 1;                // Set so breakpoints don't disturb xmission
}

void spi_xmit(Uint16 a)
{
    SpiaRegs.SPITXBUF=a;
}

void spi_fifo_init()
{
// Initialize SPI FIFO registers
    SpiaRegs.SPIFFTX.all=0xE040;
    SpiaRegs.SPIFFRX.all=0x2044;
    SpiaRegs.SPIFFCT.all=0x0;
}

void InitEPwmTimer()
{

   EALLOW;
   SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;      // Stop all the TB clocks
   EDIS;

   InitEPwm1Gpio();
   InitEPwm2Gpio();
   InitEPwm3Gpio();

   // Setup Sync
   EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;  // Pass through
   EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;  // Pass through
   EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;  // Pass through

   // Allow each timer to be sync'ed

   EPwm1Regs.TBCTL.bit.PHSEN = TB_ENABLE;
   EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE;
   EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE;

   EPwm1Regs.TBPHS.half.TBPHS = 100;
   EPwm2Regs.TBPHS.half.TBPHS = 200;
   EPwm3Regs.TBPHS.half.TBPHS = 300;

   EPwm1Regs.TBPRD = PWM1_TIMER_TBPRD;
   EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;    // Count up
   EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;     // Select INT on Zero event
   EPwm1Regs.ETSEL.bit.INTEN = PWM1_INT_ENABLE;  // Enable INT
   EPwm1Regs.ETPS.bit.INTPRD = ET_1ST;           // Generate INT on 1st event


   EPwm2Regs.TBPRD = PWM2_TIMER_TBPRD;
   EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;     // Count up
   EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;      // Enable INT on Zero event
   EPwm2Regs.ETSEL.bit.INTEN = PWM2_INT_ENABLE;   // Enable INT
   EPwm2Regs.ETPS.bit.INTPRD = ET_2ND;            // Generate INT on 2nd event


   EPwm3Regs.TBPRD = PWM3_TIMER_TBPRD;
   EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;     // Count up
   EPwm3Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;      // Enable INT on Zero event
   EPwm3Regs.ETSEL.bit.INTEN = PWM3_INT_ENABLE;   // Enable INT
   EPwm3Regs.ETPS.bit.INTPRD = ET_3RD;            // Generate INT on 3rd event

   EALLOW;
   SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;         // Start all the timers synced
   EDIS;

}

// This ISR MUST be executed from RAM as it will put the Flash into Sleep
// Interrupt routines uses in this example:
__interrupt void epwm1_timer_isr(void)
{

   // Put the Flash to sleep
   EALLOW;
   FlashRegs.FPWR.bit.PWR = FLASH_SLEEP;
   EDIS;

   EPwm1TimerIntCount++;

   // Clear INT flag for this timer
   EPwm1Regs.ETCLR.bit.INT = 1;

   // Acknowledge this interrupt to receive more interrupts from group 3
   PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}

// This ISR MUST be executed from RAM as it will put the Flash into Standby
__interrupt void epwm2_timer_isr(void)
{
   EPwm2TimerIntCount++;

    // Put the Flash into standby
	EALLOW;
    FlashRegs.FPWR.bit.PWR = FLASH_STANDBY;
	EDIS;

   // Clear INT flag for this timer
   EPwm2Regs.ETCLR.bit.INT = 1;

   // Acknowledge this interrupt to receive more interrupts from group 3
   PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}

__interrupt void epwm3_timer_isr(void)
{
   Uint16 i;

   EPwm3TimerIntCount++;

    // Short Delay to simulate some ISR Code
    for(i = 1; i < 0x01FF; i++) {}

   // Clear INT flag for this timer
   EPwm3Regs.ETCLR.bit.INT = 1;

   // Acknowledge this interrupt to receive more interrupts from group 3
   PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}

//===========================================================================
// No more.
//===========================================================================

And

//###########################################################################
//
// FILE:   DSP2803x_Spi.c
//
// TITLE:  DSP2803x SPI Initialization & Support Functions.
//
//###########################################################################
// $TI Release: F2803x C/C++ Header Files and Peripheral Examples V127 $
// $Release Date: March 30, 2013 $
//###########################################################################

#include "DSP2803x_Device.h"     // DSP2803x Headerfile Include File
#include "DSP2803x_Examples.h"   // DSP2803x Examples Include File

//---------------------------------------------------------------------------
// InitSPI:
//---------------------------------------------------------------------------
// This function initializes the SPI(s) to a known state.
//
void InitSpi(void)
{
   // Initialize SPI-A

   //tbd...

}

//---------------------------------------------------------------------------
// Example: InitSpiGpio:
//---------------------------------------------------------------------------
// This function initializes GPIO pins to function as SPI pins
//
// Each GPIO pin can be configured as a GPIO pin or up to 3 different
// peripheral functional pins. By default all pins come up as GPIO
// inputs after reset.
//
// Caution:
// For each SPI peripheral
// Only one GPIO pin should be enabled for SPISOMO operation.
// Only one GPIO pin should be enabled for SPISOMI operation.
// Only one GPIO pin should be enabled for SPICLK  operation.
// Only one GPIO pin should be enabled for SPISTE  operation.
// Comment out other unwanted lines.

void InitSpiGpio()
{

   InitSpiaGpio();
 #if DSP28_SPIB
   InitSpibGpio();
 #endif // endif DSP28_SPIB
}

void InitSpiaGpio()
{

   EALLOW;

/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAPUD.bit.GPIO16 = 0;   // Enable pull-up on GPIO16 (SPISIMOA)
//  GpioCtrlRegs.GPAPUD.bit.GPIO5 = 0;    // Enable pull-up on GPIO5 (SPISIMOA)
    GpioCtrlRegs.GPAPUD.bit.GPIO17 = 0;   // Enable pull-up on GPIO17 (SPISOMIA)
//  GpioCtrlRegs.GPAPUD.bit.GPIO3 = 0;    // Enable pull-up on GPIO3 (SPISOMIA)
    GpioCtrlRegs.GPAPUD.bit.GPIO18 = 0;   // Enable pull-up on GPIO18 (SPICLKA)
    GpioCtrlRegs.GPAPUD.bit.GPIO19 = 0;   // Enable pull-up on GPIO19 (SPISTEA)

/* Set qualification for selected pins to asynch only */
// This will select asynch (no qualification) for the selected pins.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAQSEL2.bit.GPIO16 = 3; // Asynch input GPIO16 (SPISIMOA)
//  GpioCtrlRegs.GPAQSEL1.bit.GPIO5 = 3;  // Asynch input GPIO5 (SPISIMOA)
    GpioCtrlRegs.GPAQSEL2.bit.GPIO17 = 3; // Asynch input GPIO17 (SPISOMIA)
//  GpioCtrlRegs.GPAQSEL1.bit.GPIO3 = 3;  // Asynch input GPIO3 (SPISOMIA)
    GpioCtrlRegs.GPAQSEL2.bit.GPIO18 = 3; // Asynch input GPIO18 (SPICLKA)
    GpioCtrlRegs.GPAQSEL2.bit.GPIO19 = 3; // Asynch input GPIO19 (SPISTEA)

/* Configure SPI-A pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be SPI functional pins.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAMUX2.bit.GPIO16 = 1; // Configure GPIO16 as SPISIMOA
//  GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 2;  // Configure GPIO5 as SPISIMOA
    GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 1; // Configure GPIO17 as SPISOMIA
//  GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 2;  // Configure GPIO3 as SPISOMIA
    GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 1; // Configure GPIO18 as SPICLKA
    GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 1; // Configure GPIO19 as SPISTEA

    /*
     * For SPI input to Channel 1*/
    GpioCtrlRegs.GPAPUD.bit.GPIO10 = 0;   // Enable pull-up on GPIO19 (SPISTEA)
	GpioCtrlRegs.GPAQSEL1.bit.GPIO10 = 3;
	GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 2;


    /*
     * For SPI input to Channel 2*/
    //GpioCtrlRegs.GPAPUD.bit.GPIO4 = 0;   // Enable pull-up on GPIO19 (SPISTEA)
	//GpioCtrlRegs.GPAQSEL1.bit.GPIO4 = 3;
	//GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 2;
	//*/

    /*
     * For SPI input to Channel 3
    GpioCtrlRegs.GPAPUD.bit.GPIO5 = 0;   // Enable pull-up on GPIO19 (SPISTEA)
	GpioCtrlRegs.GPAQSEL1.bit.GPIO5 = 3;
	GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 2;
	*/

    /*
     * For SPI input to Channel 4
    GpioCtrlRegs.GPAPUD.bit.GPIO11 = 0;   // Enable pull-up on GPIO19 (SPISTEA)
	GpioCtrlRegs.GPAQSEL1.bit.GPIO11 = 3;
	GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 2;
	*/

//	GpioCtrlRegs.GPAPUD.bit.GPIO10 = 0;   // Enable pull-up on GPIO19 (SPISTEA)
//	GpioCtrlRegs.GPAPUD.bit.GPIO5 = 0;   // Enable pull-up on GPIO19 (SPISTEA)
//	GpioCtrlRegs.GPAPUD.bit.GPIO11 = 0;   // Enable pull-up on GPIO19 (SPISTEA)
//	GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 0;
//	GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 0;
//	GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 0;


    EDIS;
}

#if DSP28_SPIB
void InitSpibGpio()
{
   EALLOW;

/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAPUD.bit.GPIO12 = 0;     // Enable pull-up on GPIO12 (SPISIMOB)
//  GpioCtrlRegs.GPAPUD.bit.GPIO24 = 0;     // Enable pull-up on GPIO24 (SPISIMOB)

    GpioCtrlRegs.GPAPUD.bit.GPIO13 = 0;     // Enable pull-up on GPIO13 (SPISOMIB)
//  GpioCtrlRegs.GPAPUD.bit.GPIO25 = 0;     // Enable pull-up on GPIO25 (SPISOMIB)

    GpioCtrlRegs.GPAPUD.bit.GPIO14 = 0;     // Enable pull-up on GPIO14 (SPICLKB)
//  GpioCtrlRegs.GPAPUD.bit.GPIO26 = 0;     // Enable pull-up on GPIO26 (SPICLKB)

    GpioCtrlRegs.GPAPUD.bit.GPIO15 = 0;     // Enable pull-up on GPIO15 (SPISTEB)
//  GpioCtrlRegs.GPAPUD.bit.GPIO27 = 0;     // Enable pull-up on GPIO27 (SPISTEB)


/* Set qualification for selected pins to asynch only */
// This will select asynch (no qualification) for the selected pins.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAQSEL1.bit.GPIO12 = 3;   // Asynch input GPIO12 (SPISIMOB)
//  GpioCtrlRegs.GPAQSEL2.bit.GPIO24 = 3;   // Asynch input GPIO24 (SPISIMOB)

    GpioCtrlRegs.GPAQSEL1.bit.GPIO13 = 3;   // Asynch input GPIO13 (SPISOMIB)
//  GpioCtrlRegs.GPAQSEL2.bit.GPIO25 = 3;   // Asynch input GPIO25 (SPISOMIB)

    GpioCtrlRegs.GPAQSEL1.bit.GPIO14 = 3;   // Asynch input GPIO14 (SPICLKB)
//  GpioCtrlRegs.GPAQSEL2.bit.GPIO26 = 3;   // Asynch input GPIO26 (SPICLKB)

    GpioCtrlRegs.GPAQSEL1.bit.GPIO15 = 3;   // Asynch input GPIO15 (SPISTEB)
//  GpioCtrlRegs.GPAQSEL2.bit.GPIO27 = 3;   // Asynch input GPIO27 (SPISTEB)

/* Configure SPI-B pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be SPI functional pins.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 3;    // Configure GPIO12 as SPISIMOB
//  GpioCtrlRegs.GPAMUX2.bit.GPIO24 = 3;    // Configure GPIO24 as SPISIMOB

    GpioCtrlRegs.GPAMUX1.bit.GPIO13 = 3;    // Configure GPIO13 as SPISOMIB
//  GpioCtrlRegs.GPAMUX2.bit.GPIO25 = 3;    // Configure GPIO25 as SPISOMIB

    GpioCtrlRegs.GPAMUX1.bit.GPIO14 = 3;    // Configure GPIO14 as SPICLKB
//  GpioCtrlRegs.GPAMUX2.bit.GPIO26 = 3;    // Configure GPIO26 as SPICLKB

    GpioCtrlRegs.GPAMUX1.bit.GPIO15 = 3;    // Configure GPIO15 as SPISTEB
//  GpioCtrlRegs.GPAMUX2.bit.GPIO27 = 3;    // Configure GPIO27 as SPISTEB

    EDIS;
}
#endif //endif DSP28_SPIB

//===========================================================================
// End of file.
//===========================================================================

Thanks!

  • Hello Evans,

    I haven't checked your codes carefully but based on what I see briefly, I want to confirm some thing about your SPI  connection:

    Did you connect SPISTEA pin (GPIO19) of F28027 to one of GPIO pin of F28034?

    Master (F28034) should pull-low this pin (SPISTEx) to enable SPI slave to receive the data.

    For example for Master, I use GPIO34 to connect to SPISTEA of F28027.

    So for example in main loop:

     for(;;) {

            GPIO_setLow(myGpio, GPIO_Number_34); // This pin connect to SPISTE pin of SPI slave to enable the slave

            SPI_write(mySpi, sdata);

            // Check whether the master receive ACK
            if(rdata == SLAVE_ACK)    // if master receives SLAVE_ACK = 111
            {
                sdata++;                    // Master
                asm(" NOP");
                asm(" NOP");
                rdata = 0;

                GPIO_setHigh(myGpio, GPIO_Number_34);
            }
           
            asm(" NOP");
        }

     

    Best regards,

    Maria

  • Yes in the DSP2802x_Spi.c I set:

    • GpioCtrlRegs.GPAPUD.bit.GPIO19 = 0;   // Enable pull-up on GPIO19 (SPISTEA)
    • GpioCtrlRegs.GPAQSEL2.bit.GPIO19 = 3; // Asynch input GPIO19 (SPISTEA)
    • GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 1; // Configure GPIO19 as SPISTEA

    But I don't switch it back and forth (hi to lo) like you did in your psuedocode.  I can try that later today, thank you for your response.

  • Oops sorry Maria, I didn't really answer your question.  I have connect GPIO19 on each of the 28027 to the 28034. (GPIO 10, 4, 5, & 11 from the 34 to the different 28027s)