This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DualTimeA and DualTimeB graph on the same window

Hello,

I am using DLOG module in my project. Is it possible to see DualTimeA and DualTimeB graph on the same window to see phase difference between two graph? What should be settings in CCS?

 

Regards,

 

  • Is it possible to see DualTimeA and DualTimeB graph on the same window to see phase difference between two graph?

    Same window might not be possible. But here's what you can do:

    Under Tools, select Graph then 'Dual Graphs'. In there, you can specific the starting address of the two variables you would like to plot. This generates two separate graph windows that are connected on the horizontal axis. They may appear as two tabbed window, you can select one of them and position it below the other to visually compare the graphs.

    If you would like to see dots instead of connected lines, you can right click on the graph, select 'Display Properties" , General, Display Data as "Connected Lines".

    Regards,

    Gautam