Other Parts Discussed in Thread: BOOSTXL-DRV8301, DRV8301
Hello everyone,
first my Setup:
I got a Launchpad XL (LAUNCHXL-F28027) with a BOOSTXL-DRV8301 Extension Board and a motor attached to it.
Currently I'm running Project Lab 05b with a self written SCI Extension to modify the Motor Parameters via Serial Port. Things are working as intended (finally), but the only thing which bothers me, is that whenever I got serial communication (Rx or Tx, doesn't matter) the Fault LED on the BOOSTXL-DRV8301 Board is blinking.
I already tried to modify the isr priority of sci, but that failed (I'm still a bloody beginner with these controllers).
Anyone got ideas how to overcome that?
Thanks in advance,
Patrick