Other Parts Discussed in Thread: UNIFLASH
Hello!
I am getting errors 100% of the time while trying to debug with CCS 5.5.0.00077. The problem is, it seems to be a different error every time. Also, I am using a controlCard with a Rev B part.
So far, I have restarted the PC, removed all other USB devices that use COM ports, removed and reseated the DSP card, sacrificed a goat, and even tried to use the Blinky test project.
EDIT: This issue seems to have started when I installed another device that uses FTDI drivers... is it possible that we have a driver issue? How would I check/solve this? The under "Ports" in Windows 7, Driver information is as follows:
FTDI
Date: 3/18/2011
Version: 2.8.14.0
Here is the entire console dump from about 5 min of use and maybe 2 or 3 attempts to load my program:
Cortex_M3_0: GEL Output: Memory Map Initialization Complete
Cortex_M3_0: GEL Output: Watchdog Timers Enabled
Cortex_M3_0: GEL Output: UARTs Enabled
C28xx_0: GEL Output:
Memory Map Initialization Complete
C28xx_0: GEL Output:
RAM Initialization Complete
Cortex_M3_0: Breakpoint Manager: Retrying with a AET breakpoint
Cortex_M3_0: Breakpoint Manager: Error enabling this function: Address exceeds the allowed range
Cortex_M3_0: Trouble Setting Breakpoint with the Action "Remain Halted" at 0x20004744: (Error -150 @ 0x20004744) One of the FTDI driver functions used during configuration returned a invalid status or an error. (Emulation package 5.1.232.0)
Cortex_M3_0: Trouble Reading Memory Block at 0x2000479c on Page 0 of Length 0x4: (Error -242 @ 0x0) A router subpath could not be accessed. The board configuration file is probably incorrect. (Emulation package 5.1.232.0)
Cortex_M3_0: Flash Programmer: Error erasing Sector F. Operation Cancelled.
Cortex_M3_0: Unable to terminate memory download: (Error -1003 @ 0x2BC5) Internal error: Invalid parameter passed to function. Restart the application. If error persists, please report the error. (Emulation package 5.1.232.0)
Cortex_M3_0: GEL: File: *****.out: Load failed.
C28xx_0: Error: (Error -1044 @ 0x0) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.232.0)
C28xx_0: Unable to determine target status after 20 attempts
C28xx_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
Cortex_M3_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.232.0)
Cortex_M3_0: Unable to determine target status after 20 attempts
Cortex_M3_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
Cortex_M3_0: GEL Output: Watchdog Timers Enabled
Cortex_M3_0: GEL Output: UARTs Enabled
C28xx_0: GEL Output:
Memory Map Initialization Complete
C28xx_0: GEL Output:
RAM Initialization Complete
C28xx_0: Failed CPU Reset: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.1.232.0)
C28xx_0: Trouble Reading Register PC: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.1.232.0)
C28xx_0: Trouble Reading Register ST1: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.1.232.0)
C28xx_0: GEL: Error while executing OnReset(1): Target failed to read register ST1 at (ST1&~(0x0100)) [f28m35h52c1_c28.gel:356] at C28x_Mode() [f28m35h52c1_c28.gel:31] at OnReset(1) .
C28xx_0: Error during Flash verification (Flash algorithm timed out). Operation cancelled.
C28xx_0: Flash verification returned error condition. Operation cancelled.
C28xx_0: Please make sure the memory location you are programming have not already been programmed.
CS_DAP_0: Error: (Error -241 @ 0x0) A router subpath could not be accessed. A security error has probably occurred. (Emulation package 0.0.0.0)
Cortex_M3_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.232.0)
C28xx_0: AutoRun: Target not run as breakpoint could not be set: Error enabling this function: DCU_SEL Register write failed
C28xx_0: Error: (Error -1044 @ 0x0) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.232.0)
Cortex_M3_0: Unable to determine target status after 20 attempts
Cortex_M3_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
C28xx_0: Unable to determine target status after 20 attempts
C28xx_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging