Hello,
where can I get this capacitors?
Maybe it is an error from TI, because the normal values for X7R/0402/16V ends at 100nF (Mouser, Digikey,....).
Or can I use the X5R dielectricum?
| 36 | 32 | C9-16 | 8 | 470n | CAP CER 16V 10% X7R 0402 |
|---|
Regards Uwe
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
where can I get this capacitors?
Maybe it is an error from TI, because the normal values for X7R/0402/16V ends at 100nF (Mouser, Digikey,....).
Or can I use the X5R dielectricum?
| 36 | 32 | C9-16 | 8 | 470n | CAP CER 16V 10% X7R 0402 |
|---|
Regards Uwe
Dear Gautam,
thanks for the answer, but:
Yageo have only 6,3V with 470nF (page5 of the datasheet)
Best Regards
Uwe
Yageo have only 6,3V with 470nF (page5 of the datasheet)
Yes Uwe, I did notice that. What I wanted to indicate is; have a talk with Yageo distributors. I'm sure you might get a positive feedback.
Regards,
Gautam
Uwe,
Yes, X5R can generally work as a replacement for X7R. In general, both are very similar dielectrics with the major difference being operating temperature ranges.
Because the signal across the capacitor is ~1.2V in this design, you could also comfortably move down to a 10V rating on the capacitor and still have plenty of design margin.
Thank you,
Brett