Hi:
I'm using FastRTS lib in my project,i have two question about using this lib.
1. In controlsuite ,i found that there is .asm source file in folder, can I use these source files directly, without having to include the library.
2.How do I modify the CMD file to link the FastRTS library function and function table into the RAM.
thanks!!!