I know it is a shot in the dark and that CLA and Flash are not best buddies, but I was just wondering if I can run flash erase, program and verify in CLA (for configuration data using 1 Flash sector). My configuration data is growing and it takes a whooping 1.2s to write the whole thing in flash. So far I have managed it to only do it when it is relatively "safe" in my application but it would help tremendously if I can use the CLA for it and not bother the CPU. Please confirm or deny before I dive head first into the issue. I also welcome other ideas to deal with the problem.
Thanks,
Erik