This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

No source available for "SysCtlDelay()"

I just installed CCS 6, and now when debugging I get the following message on the M3:

No source available for "SysCtlDelay() at [path to .out file]".


The code still seems to work, but I'm just wondering if this is something I need to worry about. I did not get this error message previously with CCS 5.5

I'm working on the Concerto F28M35H52C1.

Thanks