Hello,
I am creating a custom board with a 28069 (master) that is attached via SPI to a FLASH (slave).
I have been going through POSTs trying to understand if I need a GPIO to act as a chip select to the FLASH device
or if I can use the SPISTEA line. I get the impression from reading POSTs that I would need a GPIO?
Any insight would be appreciated.
Thanks,
Brent