Dear Experts,
With reference to the TI Motor Control Primer http://processors.wiki.ti.com/index.php/TMS320C2000_Motor_Control_Primer
If an application current sensing circuit (http://processors.wiki.ti.com/index.php/TMS320C2000_Motor_Control_Primer#PU_System_Model_and_Base_Values) is biased such that it assigns 3.3 V to say +15 A, and 0 V to say -10 A,
Questions:
- Would this cause a problem in the number system of the code? If there would be, is there a work around in software?
- How would the pu system work? I would still expect my +1.0 pu to be +15 A since this gives maximum output for the ADC. Is my thinking right?
- How would 0 A be interpreted, seeing that the system is not symmetric?
- Does that mean that my pu output is [-0.67 pu, +1.0 pu]
Thanks for your help!
Vincent