Dear Friends,
I'm working on PMSM Motor Control Project (with Encoder + FOC).
For that, I've imported the HVPM Sensored code (version 1.7) from control-suit. Now I've to configure the Code as per my PMSM Motor Specification and for that I've to edit in File name: HVPM_Sensored-Settings.H
Everything is working perfectly, but there is a line in HVPM_Sensored-Settings.H file,
#define BASE_VOLTAGE 236.140 // Base peak phase voltage (volt)
#define BASE_CURRENT 10 // Base peak phase current (amp)
I've checked the entire code, but no where I can find these lines.
If I want to rotate the two different PMSM Motors by using the same code,
1. PMSM Motor: Pole = 16, RPM = 165, Base Freq. = 22, Base Volt. = 24V &
2. PMSM Motor: Pole = 16, RPM = 165, Base Freq. = 22, Base Volt. = 65V
then where I've to change in the code?
How it will handle the PWM Duty Cycle to different rating Motor?
Can I set the limit of applied DC Bus Power in the code?
What should I do?