Other Parts Discussed in Thread: TMDSDOCK28335
Hi!
I am using the experimenter kit for the 28335 right now which comes with a non-isolated XDS100v2 debugger. The functionality of this debugger is sufficient for me, except that I think I require an isolated connection to the computer due to a harsh EMI environment (power application). I am aware of various options (XDS5xx, schematics for isolated XDS100v2, F37xD controlCard,..) and evaluating them right now.
One simple possible option could be to just use an usb isolator (e.g. this one: http://www.bb-elec.com/Products/USB-Connectivity/USB-Isolators/Compact-USB-Port-Guardian.aspx). However all available isolator set the USB speed to 12MBit/s.
I have seen that XDS100v2 went up to a 480MBit/s interface speed compared to v1. So two questions arise for me:
- would the XDS100v2 be able to communicate with my computer using such an isolator that sets the speed to 12mbit/s?
- Will the debugging speed actually go down (significantly)? How much more than 12MBit/s does the XDS100v2 use? Or is it more a question of delay?
Right now I normally have around 30-35 expressions in my watch window at a gobal refresh rate of 100ms. I see that the system cannot hold this refresh rate (it approximately refreshed every ~500ms). 1-2 seconds would still be okay.
Thanks!