Other Parts Discussed in Thread: DRV8301, MOTORWARE
Hi,
I am trying to run a 24V-bldc motor with DRV8301 kit, but I can't get the motor to run at its rated top speed (5200rpm). When I try it with the GUI, it will show DRV fault when the speed reaches 4900rpm. Without the GUI, the fastest speed is approx. 2290rpm, even when SpeedRef_krpm is set to 5krpm. Does anyone know what is causing the issue? where should I look into?
Thanks,
regards,
Kevin