Other Parts Discussed in Thread: CONTROLSUITE
Hi!
I'm trying to test the communication between the 2 SPIs available on Piccolo f28069. I've configured SPI-A as master and SPI-B as slave. And I've connected SPISOMIA to SPISOMIB, SPISIMOA to SPISIMOB, SPICLKA to SPICLKB, and SPISTE to SPISTE. The problem is that the program can not go into either the TX or RX interrupt of SPIB (I put breakpoints inside the interrupts). From the watch window, SpibRegs.SPIFFTX.TXFFINT=1 (always), SpibRegs.SPIFFRX.RXFFINT=0 (always). Is it because of priority problem? Here is the configuration for them:
void spi_fifo_init()
{
// Initialize SPI_A FIFO registers
SpiaRegs.SPICCR.bit.SPISWRESET=0; // Reset SPI
SpiaRegs.SPICCR.all=0x000F; //16-bit character, disable Loopback mode
SpiaRegs.SPICTL.all=0x0017; //Interrupt enabled, Master/Slave XMIT enabled
SpiaRegs.SPISTS.all=0x0000;
SpiaRegs.SPIBRR=0x0063; // Baud rate
SpiaRegs.SPIFFTX.all=0xC034; // Enable FIFO's, set TX FIFO level to 4
SpiaRegs.SPIFFRX.all=0x0034; // Set RX FIFO level to 4
SpiaRegs.SPIFFCT.all=0x00;
SpiaRegs.SPIPRI.all=0x0010;
SpiaRegs.SPICCR.bit.SPISWRESET=1; // Enable SPI
SpiaRegs.SPIFFTX.bit.TXFIFO=1;
SpiaRegs.SPIFFRX.bit.RXFIFORESET=1;
// Initialize SPI_B FIFO registers
SpibRegs.SPICCR.bit.SPISWRESET=0; // Reset SPI
SpibRegs.SPICCR.all=0x000F; //16-bit character, disable Loopback mode
SpibRegs.SPICTL.all=0x0013; //Interrupt enabled, Master/Slave XMIT enabled
SpibRegs.SPISTS.all=0x0000;
SpibRegs.SPIBRR=0x0063; // Baud rate
SpibRegs.SPIFFTX.all=0xC034; // Enable FIFO's, set TX FIFO level to 4
SpibRegs.SPIFFRX.all=0x0034; // Set RX FIFO level to 4
SpibRegs.SPIFFCT.all=0x00;
SpibRegs.SPIPRI.all=0x0010;
SpibRegs.SPICCR.bit.SPISWRESET=1; // Enable SPI
SpibRegs.SPIFFTX.bit.TXFIFO=1;
SpibRegs.SPIFFRX.bit.RXFIFORESET=1;
}
Does anybody have an idea what I'm doing wrong?
Thanks,
Lebing